Explore our latest innovations and discover SICK's success stories as one of the world's leading solutions providers for sensor-based applications. The SICK Sensor Blog helps its readers stay up to date on the latest advances in automation, ranging from production plants to processes and logistics systems. It’s time to lift the veil on the world of digital transformation.
642 results:
Result 409 - 432 out of 642
An increasing number of digital solutions are also being used in the fashion and clothing industries. The opportunities range from labeling products and presentations in stores all the way through to interaction...
Read on
Since the end of 2013, the new global standard EN ISO 14119 (Safety of machinery - Interlocking devices associated with guards - Principles for design and selection) has been taking the place of the former...
Read on
After water, tea is the worlds most consumed beverage. More than three billion cups are drunk each year in countries across the globe - the equivalent of around 450 cups per person in a year. As a beverage,...
Read on
A wide range of industrial applications in nearly all industries can be covered with 3D vision sensors. While 2D vision sensors only measure the x- and y-axes of an object, 3D vision sensors are also designed...
Read on
The impending updates to the BREF documents have indicated that mercury emissions from large combustion plants will soon have to be reduced dramatically. However, a reliable measurement solution is already...
Read on
A sensory check can mean two things in the context of ice cream. Namely, the sensual experience of the chocolate coating cracking as you bite into it, followed by the explosion of flavors. Or it can refer...
Read on
The Langenthal-based company Nencki AG is very meticulous when it comes to their bogie test stands. By using BTF08 HighLine wire draw encoders with an EtherCAT® interface and OD displacement measurement...
Read on
Counterfeit pharmaceuticals cause major financial losses, can pose health risks, and undermine patients trust. In light of this, the pharmaceuticals industry has committed itself to implementing the EU...
Read on
When it comes to metal closures in packaging, nothing can be left to chance: In products such as jam jars, the consumer goods industry requires seals to be tight and jars to be hermetically sealed. Anyone...
Read on
Thanks to the PSDI (Presence Sensing Device Initiation) function in the Flexi Soft safety controller, it is possible to control the press cycle in manual insertion presses using a type 4 safety light curtain...
Read on
One of the major issues associated with Industry 4.0 is making workflows flexible and that includes closer interaction between humans and machines. Part of this current move toward more integrated working...
Read on
At the test labs in one of the worlds largest and most cutting-edge dishwasher factories, BSH Hausgeräte GmbH has invested in a fully automated robot to conduct lifecycle tests on dishwasher panels...
Read on
FLOWSIC600-XT - the new gas flow meter from SICK seamlessly preserves its predecessors positive image as an outstanding precision measurement device for demanding industrial environments. The FLOWSIC600-XT...
Read on
Nowadays, machine and plant operators are faced with a challenging task: creating flexible production workflows with a high Level of automation while at the same time ensuring that people, machines, and...
Read on
False alarms or alarms that dont go off at all are unacceptable when it comes to protecting property or assets. The new LMS14x security 2D laser scanners provide optimum protection even in large open spaces...
Read on
Requirements for protecting machinery have changed more and more with the increasing use of automation. In the past, protective devices in the work process were something of a nuisance; for this reason,...
Read on
The ultra-mini WTB2S-2 Blue miniature photoelectric sensor takes over when conventional red-light sensors reach their limits. It can be relied upon to detect even high light-absorbing objects such as dark-blue...
Read on
In many industries, automated guided vehicles and vehicle systems are making production and logistics processes more flexible. When these vehicles have to be controlled with greater efficiency and precision...
Read on
Transparent plastic packaging, bottles made of glass or PET, ampoules, pipettes, flat, tubular, and hollow glass, films for securing loads on pallets: In many manufacturing processes, automators must cope...
Read on
Manufacturers of FMCG (Fast Moving Consumer Goods) require modern production lines to provide flexibility and modularity. Complex production and packaging processes in particular are areas in which modular...
Read on
As the follow-up to the successful FLOWSIC600, the FLOWSIC600-XT ultrasonic gas flow meter is setting new standards in its market segment. With four device variants available, the FLOWSIC600-XT can take...
Read on
With its latest solution - a shaftless platform lift - Ascendor is offering an affordable elevator model for private households. Rugged laser sensors from SICK protect the freely accessible area under...
Read on
Industrial production in the future will see us working with assistants that are modular, versatile and, above all else, mobile. In KMR iiwa, KUKA Roboter GmbH has developed a fully automated, autonomous...
Read on
Even at the development and design stage of a machine, it is important to consider how it will ensure safety - all too often, accidents are the result of a failure to carry out adequate risk assessments...
Read on
Result 409 - 432 out of 642
Please wait a moment...
Your request is being processed and may take a few seconds.