SICK Sensor Blog

SICK Sensor Blog
SICK Sensor Blog

Explore our latest innovations and discover SICK's success stories as one of the world's leading solutions providers for sensor-based applications. The SICK Sensor Blog helps its readers stay up to date on the latest advances in automation, ranging from production plants to processes and logistics systems. It’s time to lift the veil on the world of digital transformation.

Filter articles

642 results:

Result 505 - 528 out of 642

Whether its the Watchman, Optotrap OTD or PLS - SICK represents innovation in laser scanner development. SICK has been working in the field of laser scanners for nearly 40 years and recognized early that... Read on
On the path to establishing networked production processes, the focus up to now has been on optimizing physical production and logistics processes. Thanks to the latest IT technologies, it is now possible... Read on
The machine vision specialist, IVP AB, was founded more than 25 years ago in the university city of Linköping in southern Sweden as an offshoot of the university there. Since then, the company has... Read on
With respect to long travel distances of aisle stackers in conjunction with safe speed monitoring, it is essential to ensure steady, fast, and above all, low-noise output of measured values to the controller... Read on
When it comes to integrating sensors into industrial fieldbuses, every industry has its own individual requirements. This is why there are more than two dozen industrial communication systems available... Read on
With the construction of the most advanced car tower in Switzerland, the Züri West car dealership in Schlieren can now offer its customers a very special shopping experience. At the press of a button,... Read on
The new DT50-2 Pro distance sensor from SICK provides the perfect combination of measurement performance and size. Based on the patented HDDM™ time-of-flight technology it provides precise and reliable... Read on
Open the door, load the dirty dishes, add detergent, and restart the cycle: dishwashers have to complete hundreds of challenging test cycles before they can be relied upon to perform in day-to-day operation... Read on
52 dip tanks with 80 approach positions fed by three automatic carriages. That's exactly what printed circuit board specialist Varioprint AG based in Heiden, Switzerland, has been benefitting from in recent... Read on
In the case of industrial trucks with a driver's seat, accidents involving a collision with people, other trucks, warehouse facilities or structural elements can be identified as the cause for approximately... Read on
Imagine a sensor that can let you know when something is about to malfunction: The IO-Link technology offers a diverse range of options for cost-effective, bidirectional communication between sensors and... Read on
As a leading transmission system operator for regenerative energies in Europe, Amprion GmbH operates the most extensive high-voltage transmission system measuring some 11,000 km (6,800 miles) between Lower... Read on
MLG-2 is the new generation of intelligent automation light grids from SICK. The product family sets a new standard in terms of resolutions, response times, evaluation options and ease of use. The MLG-2... Read on
SICK's reliable and user-friendly W11-2 and W4-3 photoelectric sensors help Swiss trading company Avesco AG to provide a fast delivery service for construction machinery components. SICK's photoelectric... Read on
ARBURG is a global leader in the manufacture of high-quality injection molding machines. The company was searching for a solution that would identify incorrectly positioned inserts, preventing the production... Read on
The French regional transport operator RATP has completed a project investigating the rolling characteristics of its regional trains. The aim of the project was to identify rail wear zones in order to... Read on
Actemium Logistics provides automated solutions such as picking, conveying and sorting, WMS integration for companies working in logistics. As a means of securing access to a palletizing system for E... Read on
Drivers are familiar with winding around annoying curves in the parking garage until finally sighting an open spot. If the driver has a plane or train to catch, this can be especially unpleasant. This... Read on
From laser-based bar code scanners and high-end solutions with 2D cameras to RFID technology: SICK is synonymous with years of know-how and experience in all automatic identification technologies. This... Read on
Every year in the Swiss Alps you can hear the sound of debris flows with thousands of tonnes of detritus rushing down into valleys, and towards endangered transportation routes and settlements. The Swiss... Read on
The Tele2 Arena in Stockholm is a stadium with a retractable roof. The benefit for spectators in the stadium and television viewers: There are no shadows on the playing field, when the roof is fully... Read on
Measuring the oxygen in the process can be quite simple. The TRANSIC100LP from SICK is the rugged transmitter that uses Tunable Diode Laser Spectroscopy (TDLS) to measure O2 reliably. A technology more... Read on
Clothes make the man, so says the proverb - but only if they fit. Despite the vast number of available sizes, it is sometimes difficult to find a shirt, pants, a dress or a skirt that fits perfectly. Custom-made... Read on
Frozen fish specialties are a solid alternative to fresh fish.  But where was the fish caught? And how?  Femeg, a German producer of frozen fish specialties, has the answer: QR codes on frozen... Read on

Result 505 - 528 out of 642