Automation in intralogistics: Perfecting the automated forklift truck

2022-10-11

Logistics automation is on the rise. Whether due to digital transformation, the global pandemic, or the general focus on a higher degree of automation – intelligent intralogistics is turning into more than just a trend. A crucial factor here is state-of-the-art automated guided vehicle solutions. To meet the diverse challenges of transporting goods, VisionNav Robotics, a global provider of autonomous vehicles, and SICK are providing a whole range of joint solutions.

To meet the diverse challenges of transporting goods, VisionNav Robotics, a global provider of autonomous vehicles, and SICK are providing a whole range of joint solutions.
To meet the diverse challenges of transporting goods, VisionNav Robotics, a global provider of autonomous vehicles, and SICK are providing a whole range of joint solutions.

The combination of VisionNav Robotics forklift technology with intelligent sensor technology plus the many years of experience of SICK enables the use of forklift trucks in demanding environments, such as automatic navigation, safe and effective avoidance of obstacles or shelf detection, to name a few examples.

 

The various sensor solutions for the forklift truck: for safety and efficiency in operation

But how exactly do these sensors on the forklift truck work? What new applications are possible for the forklift truck? The video shows how the sensor solutions used in very different places for different tasks ensure safe and highly efficient operation of the forklift trucks:

The TiM351 2D LiDAR sensor is used in the VNE20 counterbalanced truck for indoor and outdoor use, which does loading work. It ensures reliable avoidance of obstacle, thereby increasing safety, especially in demanding environments.

激光扫描仪传感器
紧凑型 2D LiDAR 激光扫描仪 - 具有成本效益且性能强大
TiM
The TiM351 2D LiDAR sensor ensures reliable avoidance of obstacle, thereby increasing safety, especially in demanding environments.
The TiM351 2D LiDAR sensor ensures reliable avoidance of obstacle, thereby increasing safety, especially in demanding environments.

The TiM561 2D LiDAR sensor is used in the VNP15 automated counterbalanced truck for mesh box transport in warehouses with limited space. This ensures that the position of the pallets is accurately detected and that the forks of the truck are correctly inserted into the pallet.

The TiM561 2D LiDAR sensor ensures that the position of the pallets is accurately detected and that the forks of the truck are correctly inserted into the pallet.
The TiM561 2D LiDAR sensor ensures that the position of the pallets is accurately detected and that the forks of the truck are correctly inserted into the pallet.

VisionNav Robotics uses the PFG19 wire draw encoder in the VNR14 automated reach truck for access to shelves in high-bay warehouses; this encoder allows the truck to monitor the lift height of the forks in real time. At the same time, a Dx35 mid-range distance sensor is used to measure the sideshift of the forks and control it with millimeter precision. The UM30 ultrasonic sensor controls the forklift’s height protection function, and an inductive proximity sensor (IME) helps detect target positions. Finally, the DBS36/50 incremental encoder measures the angle of the drive unit on the wheel of the forklift.

The Dx35 mid-range distance sensor controls the sideshift of the forks, and the UM30 ultrasonic sensor controls the forklift’s height protection function.
The Dx35 mid-range distance sensor controls the sideshift of the forks, and the UM30 ultrasonic sensor controls the forklift’s height protection function.
增量型编码器
用于工业应用的紧凑型标准增量型编码器
DBS36/50
拉线编码器
适用于室内外区域的超小型精密拉线编码器
EcoLine
激光距离传感器
在应用时显示正确大小 – 灵活测量或可切换至 35 m
Dx35
电感式接近传感器
适合工业环境的经济型电感式标准传感器
IME
超声波距离传感器
通用的问题解决方案
UM30

 

If CE marking of the automated forklift truck is required, the nanoScan3 safety laser scanner with the Flexi Soft safety controller ensures the vehicle and its surroundings are safe.

安全控制器
可使用软件编程的安全控制器
Flexi Soft
安全激光扫描仪
SICK 最小的安全激光扫描仪——正确高效、坚固可靠
nanoScan3

 

Higher storage capacity and reduction of damage in the warehouse

This is how sensor solutions from SICK guarantee that automated forklift trucks perform their tasks reliably, thereby increasing efficiency and safety in different logistics operations. This leads to a higher storage capacity and at the same time to a significant reduction in goods damage in the warehouse. Logistics automation continues to advance – and with it the two partners VisionNav Robotics and SICK.

About VisionNav Robotics

VisionNav Robotics was co-founded by a team of PhD students at the Chinese University of Hong Kong. The company focuses on the application of key technologies such as artificial intelligence, environment awareness, deep learning or servo control in the field of autonomous driving in industry. VisionNav offers automated vehicles and flexible autonomous logistics solutions for production lines and warehouse logistics.

 

Read more

Hybrid approaches increase efficiency in production and logistics

Read more

Autonomous intralogistics from indoors to outdoors: SICK and Stäubli WFT provide a seamless logistics chain for BASF

Read more

Greater autonomy thanks to modular vehicle fleet: Seamless indoor and outdoor operation in intralogistics

Read more

Jungheinrich automates lift trucks: higher throughput through agile cornering and safety

Read more

移动机器人:
Move into new dimensions

无论是在生产领域、物流领域还是服务领域,机器人技术都在不断发展。适用于各类型移动机器人的传感器解决方案

了解更多